Technical FAQs

Ask a Question

Are the LC frame breakers rated for DC voltage?

No. The LC breakers were not tested or rated for DC voltage. Instead, use an LA type breaker, which is rated up to 250VDC, or LH frame breaker which is rated up to 500VDC.


CTA-ID : 2044579
Was this helpful?
What can we do to improve the information ?