Technical FAQs

Ask a Question

On a QUM400CK, what is the specified torque requirements for the incoming (line side) phase and neutral lugs?

The incoming line phase and neutral lugs are purchased separately and field installed. Only Anderson VERSA-CRIMP compression lugs VHCL-600-12BN and VHCL-750-12BN are listed for use with this device. Compression lugs do not have a torque requirement associated with them. With either lug used, the lug mounting nut should be torqued to 300 LB-IN. This information is documented on the device`s wiring diagram.



CTA-ID : 2044566
Was this helpful?
What can we do to improve the information ?