Technical FAQs

Ask a Question

What are the repair parts for a PAK76C, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161
Interior Trim - 4054024201
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4054022350 (Obsolete - replaced by 4054022351) and (2) 4054009150 (Includes the Base Assy, Circuit Breaker(s) and Receptacle(s) listed below)
Base Assembly - 4054006850
Circuit Breaker - QO120GFI and QO2505212
Receptacle - 4054001450 (125 volt/20 amp) and 4053901901 (Obsolete - replaced by 4054027950) (125/250 volt/50 amp)
Neutral Bonding Screw - 4054017250
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2044752
Was this helpful?
What can we do to improve the information ?