Technical FAQs

Ask a Question

Is a factory or field installed normally closed alarm switch available for the older N frame breakers?

There is no normally closed (NC) alarm switch available for the N frame breaker. A normally open (NO) alarm switch is available factory installed using suffix 2100. Or, a field installed normally open alarm switch is available using catalog number NA12100.


CTA-ID : 2044291
Was this helpful?
What can we do to improve the information ?