Technical FAQs

Ask a Question

Does the QUM400CL meet EUSERC specifications?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices 

Environment:
Utility specifications

Cause:
Installation 

Resolution
The QUM400CL device does not meet EUSERC specifications. However, some EUSERC member utilities may allow it to be used. The utility company should be contacted for their approval before purchasing or installing this device.


CTA-ID : 2044539
Was this helpful?
What can we do to improve the information ?