Technical FAQs

Ask a Question

Can a Model 6 Motor Control Center be obtained with an epoxy based paint finish?

Issue:
Can a Model 6 Motor Control Center be obtained with an epoxy based paint finish?

Product Line:
Model 6 motor control center.

Environment:
Product features.

Cause:
Product features.

Resolution:
No. Square D/Schneider Electric does not offer epoxy paint finishes for Motor Control Centers. The standard paint type is electrodeposited ANSI #49 paint on standard steel enclosures. Other color paints may be requested, and will be applied over the ANSI 49 finish.


CTA-ID : 2044661
Was this helpful?
What can we do to improve the information ?