Technical FAQs

Ask a Question

What are the repair parts for the SC2636M225FPV, Series M01?

Issue:
Design Repair parts

Product Line:
Combination Service Entrance Devices

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4053442852
Meter Cover Mounting Screw - 4020513001K (This kit contains 10 screws, but only one screw is required to secure the cover)
Branch Wiring Gutter Cover (Below Meter Cover) - 4056178101
Branch Wiring Gutter Cover Mounting Screw - 404020513001K (This kit contains 10 screws, but only one screw is required to secure the cover)
Utility Pullbox Cover - 4056181150 (Includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056184050 (Includes hinges)
Load Center Cover Mounting Screws - (2) 2142217101
Dead Front Interior Trim - 7329420401
Dead Front Interior Trim Mounting Screw - 4020513001K (This kit contains 10 screws, but only two screws are required to secure the interior trim)
Load Center Interior - 7329490850 (Does not include main breaker or current transformer connector assemblies)
Load Center Interior Mounting Screw - (8) 4020510001
Main Breaker - QOM2225VH
Current Transformer Connector Assembly - (2) 7329451150 and (4) 2342702001 mounting keps nuts.
Meter Base - 4054102503 (Phenolic Base only - does not include line and load phase jaws, see below. If 5th jaw is required order catalog number 5J)
Meter Base Mounting Screw - 2142717200
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850)
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Meter Sealing Ring - 2920910001
Left Line Side Phase Lug - 4025116051
Left Line Side Phase Lugs Mounting Bolt - 2271020242
Left Line Side Phase Lugs Mounting Keps Nut - 2342702001
Right Line Side Phase Lug and Line Side Neutral Lug are not field repairable.
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE


CTA-ID : 2044763
Was this helpful?
What can we do to improve the information ?