Technical FAQs

Ask a Question

Are EZ Meter-Pak Main devices suitable for either top or bottom feed applications?

Issue:
EZM Mains Wiring Configurations
 
Product Line:
EZ METER-PAK Metering Equipment - EZM

Environment:
Line Side Cable and Conduit Entry

Cause:
Available Entry Points for Line Side Feeds to EZM Mains

Resolution:
EZM Mains are available in three Styles: Main Circuit Breakers, Main Fusible Switches and Main Lugs Tap Boxes.
Line Side Cable and Conduit Entry to these Mains are available in three different configurations: Overhead Feed Only, Underground Feed Only, and Combination Overhead or Underground Feed.
NOTE: EZM Meter Centers installed outdoors (NEMA 3R) requires use of Liquid Tight or Water Tight Hubs or Fittings when entering or exiting any Enclosure above live parts.
 
The following EZM Mains are configured for OVERHEAD Feed Only:
       Main Circuit Breakers                                Main Fusible Switch                    Main Lugs Tap Boxes           
EZM11200GCBT#* EZM31200GCBT#*                  ------                  ------                  ------                 ------
EZM11200JCBT#* EZM31200JCBT#*        EZM11200FST#*  EZM31200FST#*       ------                 ------           
#  TOP Entry Only Main Device
*  Supplied with Driphood (NEAM 3R) removable for indoor use, and a Top Indoor Endwall supplied with a removable Insert.
 
The following EZM Mains are configured for UNDERGROUND Feed Only:
       Main Circuit Breakers                                 Main Fusible Switch                          Main Lugs Tap Boxes                   
EZM1400CBU        EZM3400CBU             EZM1400FSU        EZM3400FSU        EZM1400TBU        EZM3400TBU     
EZM1600CBU        EZM3600CBU             EZM1600FSU        EZM3600FSU              ------                       -------     
EZM1800CBU        EZM3800CBU             EZM1800FSU        EZM3800FSU        EZM1800TBU        EZM3800TBU     
EZM11000CBU      EZM31000CBU                   ------                      ------                      ------                        ------
    ------                           ------                           ------                      ------               EZM11200TBU      EZM31200TBU
EZM11200GCBU*  EZM31200GCBU*               ------                      ------                     ------                         ------
EZM11200JCBU*   EZM31200JCBU*         EZM11200FSB*    EZM31200FSB*           ------                         ------
EZM11200GCBE*   EZM31200GCBE*             ------                       ------                      ------                        ------
EZM11200JCBE*   EZM31200JCBE*        EZM11200FSE*     EZM31200FSE*            ------                       ------
EZM11600GCBU    EZM31600GCBU               ------                       ------                      ------                       ------
EZM12000CBU      EZM32000CBU                  ------                       ------                      ------                       ------              
*  Supplied with Driphood (NEAM 3R) removable for indoor use, and a Top Indoor Endwall supplied with a removable Insert.
 
The following EZM Mains are configured for Combination of OVERHEAD or UNDERGROUND Feed:
       Main Circuit Breakers                              Main Fusible Switch                              Main Lugs Tap Boxes         
    ------                         ------                           ------                       ------                 EZM1225TB          EZM3225TB
EZM1400CB            EZM3400CB              EZM1400FS          EZM3400FS          EZM1400TB          EZM3400TB
EZM1600CB            EZM3600CB              EZM1600FS          EZM3600FS          EZM1600TB          EZM3600TB
EZM1800CB            EZM3800CB              EZM1800FS          EZM3800FS          EZM1800TB          EZM3800TB
EZM11000CB          EZM31000CB             EZM11000FS        EZM31000FS            ------                       ------
        ------                     ------                            ------                      ------                EZM11600TB        EZM31600TB
EZM11600GCBC     EZM31600GCBC              ------                      ------                     ------                       ------
EZM11600JCBC      EZM31600JCBC               ------                     ------                      ------                       ------
EZM12000CB          EZM32000CB                   ------                      ------               EZM12000TB        EZM32000TB   



CTA-ID : 2044770
Was this helpful?
What can we do to improve the information ?