Technical FAQs

Ask a Question

What is the wire range for the main lugs in a 400a NQOD panel ?<br /><br />

The lug range is (2) #1/0-300MCM or (1) #1/0-750MCM AL or CU.

REFER TO PAGE 9-8 OF THE 174 DIGEST




CTA-ID : 2044451
Was this helpful?
What can we do to improve the information ?