Technical FAQs

Ask a Question

What is the catalog number for the flange mounting bolts for LJ wireway that connects two sections together?

There is no kit available to obtain flange mounting bolts. However, wireway sections may be easily bolted together by using standard hardware store 1/4-20 x 1`` screws/bolts. Or the customer may order an extra connector kit which contains the mounting bolts.


CTA-ID : 2043797
Was this helpful?
What can we do to improve the information ?