Technical FAQs

Ask a Question

What is the mounting depth range of the9422ARP11?

6.38`` to 17.88`` from the surface of the outside of the enclosure where the handle operator mounts to the back pan where the circuit breaker mounts.


CTA-ID : 2042172
Was this helpful?
What can we do to improve the information ?