Technical FAQs

Ask a Question

What are the insulation systems and average temperature rise ratings of the 9070 Type T and TF control transformers?

The information provided herein relates to the ``Type I`` dimension key breakdown by VA.  
The Insulation System <> Avg. Temperature Rise of 9070 Type T and TF, Type I dimension key are:
25 to 150 VA -- Class 105 <> 50 deg C rise
200 to 350 VA -- Class 130 <> 80 deg C rise
500 to 5000 VA -- Class 180 <> 115 deg C rise


CTA-ID : 2041999
Was this helpful?
What can we do to improve the information ?