Technical FAQs

Ask a Question

What are the input voltage ranges on an voltage applied counter catalog number RC87610150?

Terminals 4, 5, and 6 are the input terminals. Terminals 4 and 5 will accept an input voltage range of 5- 50V AC or DC , and terminals 5 and 6 will accept an input voltage range of48V-240V AC. Terminals 1,2 and 3 are the reset terminals. You apply 48 to 240 volts AC on terminals 1 and 2, and a voltage of 5 to 50 volts AC ar DC on terminals 2 and 3 to reset.

CTA-ID : 2041797
Was this helpful?
What can we do to improve the information ?