Technical FAQs

Ask a Question

What Main Lug Kit is required to convert a Convertible Main, Main Breaker QO or HOMELINE Load Center to a Main Lugs Load Center?

Issue:
Selection

Product Line:
QO and HOMELINE LC

Cause:
Convert MB to MLO

Resolution:
For QO or HOMELINE Main Breaker, Convertible Main Load Centers with 100A or 125A QOM1-VH main breakers, use QOL125. If the main breaker knockout has been removed from the trim, also order QOM1FP filler plate 

For QO or HOMELINE Main Breaker, Convertible Main Load Centers with 150A, 200A or 225A QOM2-VH main breakers, use QOL225. If the main breaker knockout has been removed from the trim, also order QOM2FP filler plate 




CTA-ID : 2041858
Was this helpful?
What can we do to improve the information ?