Technical FAQs

Ask a Question

What is the AIC rating of the single pole FY type breakers?

FY breakers have a 14k AIC rating at 240V or 277V. They are for use on 208Y/120V or 240/120V or 480Y/277V systems.

CTA-ID : 2041847
Was this helpful?
What can we do to improve the information ?