Technical FAQs

Ask a Question

What is the terminal lug data for the QO2000NS?

The terminal lug wire range is #4 to 2/0 Aluminum or Copper AWG.
The neutral terminals accept #12 - #1 Al or #14 - #1 Cu.
The grounding terminals accept #12 - #2 Al or #14 - 2 Cu.


CTA-ID : 2041832
Was this helpful?
What can we do to improve the information ?