Technical FAQs

Ask a Question

Can an EZM 3-Phase, 4-Wire Meter Center be fed from a 1-Phase, 3-Wire remote mounted Service Disconnect?<br />

No, A 3-Phase, 4-Wire EZM Meter Center may not be fed from an upstream 1-Phase, 3-Wire Service Disconnect.
Refer to Digest 174, Page 2-9 for additional information.


CTA-ID : 2041953
Was this helpful?
What can we do to improve the information ?