Technical FAQs

Ask a Question

What is a QO140M200EP, QOC40UFL, HOM3040M200CEP, HOMC30UFL, or EWPLATE?

Issue:
Product design features

Product Line:
QO and Homeline load centers

Environment:
Catalog number descriptions

Resolution:

Here is a brief description of the above products:
QO140M200EP - QO, 40-space, 40-circuit, 1-phase, 200A, main breaker load center, with end-plates feature. There are 4 End-plates included (2 different KO configurations). The Cover is not included.
QOC40UFL - Extra-long QO cover for hiding drywall cuts.
HOM3040M200CEP - HOM, 30 space, 40 circuit, 1 phase, 200A, main breaker load center with end-plates feature. There are 4 End-plates included (2 different KO configurations). There is a Standard-length cover included.
HOMC30UFL - Extra-long HOM cover for hiding drywall cuts.
EWPLATE - Replacement parts kit consisting of 4 ``end-plates`` for use on above load centers.
FOR ADDITIONAL INFORMATION - Call 1-888-SQUARED, and ask to speak to Lexington Product Support Group.



CTA-ID : 2041787
Was this helpful?
What can we do to improve the information ?