Technical FAQs

Ask a Question

What is the short circuit current rating for the DTU224NRB Series E1?

Issue:
Application

Product Line:
Double Throw Safety Switch

Cause:
Clarifying short circuit current rating

Resolution:
This switch is suitable for use on a circuit capable of delivering not more than 10,000 rms symmetrical A, 240 V~ maximum when protected by class H or class K fuses rated 200 A maximum.




CTA-ID : 2041328
Was this helpful?
What can we do to improve the information ?