Technical FAQs

Ask a Question

What is the maximum number of spaces and circuits the CQO124M125C60, Series S04, load center will accept?

Issue:
Product design features

Product Line:
Canadian QO load centers

Environment:
maximum circuits

Cause:
Application

Resolution:
The maximum number of spaces is 24 using standard QO 1-pole breakers and the maximum number of circuits is 48 using tandem QO branch breakers. 

 
Was this helpful?
What can we do to improve the information ?