Technical FAQs

Ask a Question

Is breaker space on the bus required to feed the surge supression circuits on a NQ442L2TVS212C panelboard interior?

No. The surge suppression units are fed from the bus on this interior. There is no need to allow space on the bus for a two pole breaker to feed the suppression section.


CTA-ID : 2041647
Was this helpful?
What can we do to improve the information ?