Technical FAQs

Ask a Question

Can a QO single pole breaker work at 24 VAC?

Yes. The QO single pole breaker is rated at 120V, but can be used at lower voltages.


CTA-ID : 2041747
Was this helpful?
What can we do to improve the information ?