Technical FAQs

Ask a Question

Which end is the input, and which end is the output on Multi-9 type breakers? Can Multi-9 breakers be backfed?

By convention, the ``on`` end or top of the breaker is the line or input side. The ``off`` or bottom end of the breaker is the load or output side. However, Multi-9`s can be also be backfed, in which this convention is reversed.


CTA-ID : 2041717
Was this helpful?
What can we do to improve the information ?