Technical FAQs

Ask a Question

Can the QO342MQ150 3-phase Load Center be ordered with a 100A main circuit breaker or any other size main breaker, instead of the 150Amp?

Product features

Product Line:
QO load centers

Main Breaker Ampere rating


Yes, the Catalog number would be a special order catalog number - QO342MQ225100. The List pricing would be the same as the standard catalog number.  

Also, other Main Breaker sizes could be ordered as long as they are LESS THAN 150amp, which is the maximum ampere rating of this load center.

CTA-ID : 2041519
Was this helpful?
What can we do to improve the information ?