Technical FAQs

Ask a Question

On a H365 switch what is the dimension of switch with the handle extended 90 degrees.

22 inches. From the rear of enclosure to the pivot point of the switch handle it is 10``, and the handle is 12`` long.

CTA-ID : 2041322
Was this helpful?
What can we do to improve the information ?