Technical FAQs

Ask a Question

Is the DTU224NRB double throw Safety switch suitable for use as service equipment?

Issue:
Application

Product Line:
Double Throw Safety Switch

Cause:
Application

Resolution:
Yes, this switch is marked "suitable for use as service equipment". The neutral should be bonded to the enclosure with the neutral bonding screw provided with the switch. 


CTA-ID : 2041640
Was this helpful?
What can we do to improve the information ?