Technical FAQs

Ask a Question

Does Square D offer a Series D2, 400amp Fusible Switch similar to the QMB3400LA breaker device?

Issue:
Product Availability

Product Line:
QMB Swithes

Environment:
400amp Fusible unit

Cause:
Application

Resolution:
No, Square D does NOT offer a Fusible QMB, 400Amp Series D2 switch for use with the OLD pre-series E QMB panelboards. The maximum fusible Series D2 switch is 200amp.



CTA-ID : 2041308
Was this helpful?
What can we do to improve the information ?