Technical FAQs

Ask a Question

What are the replacement parts for the P1200R, series A01?

Issue:
Current design repair parts

Product Line:
Enclosed Circuit Breakers

Environment:
Repair parts

Cause:
Maintenance

Resolution:

Following are the replacement parts for the P1200R, series A01. No other parts are available.

ENCLOSURE COVER ASSEMBLY  - P1200RC (This assembly is the large cover on the front of the enclosure, onto which these items are installed: Rainproof Breaker Cover and housing, handles, lower support bracket, and cover latch. A quantity of 8 Cover Mounting Screws are also included.)
RAINPROOF BREAKER COVER - 4051595150 (This is the small, hinged cover over the circuit breaker, onto which these items are installed: 2 hinges and 1 latch. It does not include the housing.)
COVER MOUNTING SCREWS - 4051595350 (Order qty 1 = bag of 9 screws)


CTA-ID : 2041617
Was this helpful?
What can we do to improve the information ?