Technical FAQs

Ask a Question

What is the maximum number of circuits that you can get in a CQO132M200C, Series S-04, load center?

The maximum number of circuits using standard QO breakers is 32 circuits. If you use tandem QO breakers the panel is approved for up to 64 circuits.

CTA-ID : 2041567
Was this helpful?
What can we do to improve the information ?