Technical FAQs

Ask a Question

Why are the 8903 type L lighting contactors available from factory with 10 or 12 normally closed contacts but for field conversion you are restricted to 8 normally closed contacts ?

The 8903 L contactor is factory modified to accomodate the 10 or 12 normally closed contacts. This modification is not something that can be accomplished in the field. These contactors are only available with 120v coils.


CTA-ID : 2041537
Was this helpful?
What can we do to improve the information ?