Technical FAQs

Ask a Question

How does one select overload thermal units for the Part Winding Starter?

The 6-thermal units are selected on the basis of the full load current of each winding, normally 1/2 the total amp rating of the motor.

CTA-ID : 2041368
Was this helpful?
What can we do to improve the information ?