Technical FAQs

Ask a Question

The Masterpact NW product selector makes you select top or bottom feed when ordering metering CT`s. Does this mean that the NW is marked Line & Load and cannot be reversed fed?

The Masterpact NW can be reversed fed. The metering CT`s are located in a difficult to reach position on the back of the breaker. The decision was made to ask whether the breaker was top or bottom feed so that the metering CT can be properly wired on the manufacturing line before the presence of other assemblies make installation difficult.

CTA-ID : 2041100
Was this helpful?
What can we do to improve the information ?