Technical FAQs

Ask a Question

Are NEMA 1 enclosures available separately for the 8911DPSO starters?

Yes, select based on device to be enclosed:

Class 8911 Type DPSO 20 through 40 amp use 9991DPSG1.
Class 8911 Type DPSO52 & DPSO53 use 9991DPSG2.
Class 8911 Type DPSO63, DPSO73 & DPSO93 use 9991SEG8
These enclosures also include the external reset button.


CTA-ID : 2041317
Was this helpful?
What can we do to improve the information ?