Technical FAQs

Ask a Question

What are the replacement parts for the P1200S, series A01?

Issue:
Current design repair parts

Product line:
Circuit Breaker Enclosures

Environment:
repair parts

Cause:
Maintenance

Resolution:

Following are the replacement parts for the P1200S, series A01. No other parts are available.
NO LABELS ARE INCLUDED ON ANY OF THE BELOW PARTS.

ENCLOSURE REPLACEMENT COVER ASSEMBLY -  P1200SC (This assembly is the large cover for the front of the enclosure, which contaings the following parts: Breaker Closing Plate, handles, lower support bracket, and cover latch. A quantity of 8 Cover Mounting Screws are also included.)
NOTE: The above replacement cover does NOT include the Nameplate or any other labels and the Nameplate is NOT available as a repair part.

BREAKER CLOSING PLATE - 4051595250 (This is the small cover installed over the opening for the circuit breaker. A quantity of 4 mounting screws are also included.)
COVER MOUNTING SCREWS - 4051595350 (order qty 1 = bag of 9 screws)


 
Was this helpful?
What can we do to improve the information ?