Technical FAQs

Ask a Question

Is there an electrical interlock kit for use with the 9422 CSF30 flexible cable mechanism for Merlin Gerin NSF circuit breakers?

No, we do not offer a standard 9999 electrical interlock kit; however, we offer instead an auxiliary switch, cat. no. 29450, which will field install into the case of the circuit breaker and will perform the same function.

CTA-ID : 2041603
Was this helpful?
What can we do to improve the information ?