Technical FAQs

Ask a Question

What is the current consumption for the XB4 and XB5 protected LED`s?

Applicable to all colors:
24Vac/dc supply blocks: 18mA
120Vac supply blocks: 14mA.
240Vac supply blocks: 14mA


CTA-ID : 2041862
Was this helpful?
What can we do to improve the information ?