Technical FAQs

Ask a Question

The GCDSP reads ``Checksum Error``. Is this a problem with the relay?

This is an issue with the display module, not the relay. It was corrected in 2004. Replace the GCDSP module.


CTA-ID : 2041202
Was this helpful?
What can we do to improve the information ?