Technical FAQs

Ask a Question

What is the maximum number of circuits that you can get in a CQO140M125C125, Series S04, load center?

The maximum number of circuits using standard QO breakers is 40 circuits. If you use tandem QO breakers the panel is approved for up to 54 circuits.

CTA-ID : 2041568
Was this helpful?
What can we do to improve the information ?