Technical FAQs

Ask a Question

What is the maximum number of circuits that you can get in a CQO140M200C, Series S04, load center?

Issue:
Product Design

Product Line:
Canadian QO LC

Cause:
Clarification

Resolution:
This load center has 40 spaces available for up to 80 circuits. The maximum number of circuits using standard full size QO breakers is 40 circuits. If you use tandem QO breakers the panel is approved for up to 80 circuits.


CTA-ID : 2041562
Was this helpful?
What can we do to improve the information ?