Technical FAQs

Ask a Question

Is a local current meter kit / trip indicator standard or optional on a LX, MX, NX, or PX breaker?

The ALAM ammeter for LX, MX, NX breakers is optional and needs to be ordered separately. The ammeter for the PX is ALAMP. These are standard on LE, ME, NE, and SE circuit breakers.


CTA-ID : 2041178
Was this helpful?
What can we do to improve the information ?