Technical FAQs

Ask a Question

What are the dimensions of the QO342L225G load center?

Issue:
Dimensions

Product Line:
QO Load Center

Cause:
Dimensions

Resolution:
The QO342L225G is 37.98" H x 14.25" W x 3.75" D. 
Click this link to access the Approval Drawing #3037:
http://static.schneider-electric.us/docs/Electrical%20Distribution/Load%20Centers/QO%20Three%20Phase%20Load%20Centers/3037.pdf

The drawing is also attached for your reference. 



CTA-ID : 2042437
Was this helpful?
What can we do to improve the information ?