Technical FAQs

Ask a Question

What is the catalog number for the Equipment Grounding Kit for the H361-2AWK, Series F6?

The H361-2AWK, Series F6, contains equipment grounding lugs factory installed. There are two lugs provided, each capable of terminating (1) #14-2 CU or (1) #12-2 AL, or (2) #14-10 CU or (2) #12-10 AL.

CTA-ID : 2041207
Was this helpful?
What can we do to improve the information ?