Technical FAQs

Ask a Question

What is the spacing between the mounting holes on a flush plate catalog number 9001K25?

The mounting holes are 1.38`` from the sides, 3 9/32`` apart. They are spaced at standard wall box distance.

CTA-ID : 2043261
Was this helpful?
What can we do to improve the information ?