Technical FAQs

Ask a Question

Can a three pole breaker be used on a single phase (two-wire) load in a three phase panel?

Issue:
Product design

Product Line:
Molded Case Circuit Breakers

Cause:
Application

Resolution:
Yes.According the UL White Book (Product Category DIVQ), multipole common trip circuit breakers rated 125/250V are suitable for use for a single-phase multiwire circuit, with or without the neutral connected to the load. Courtesy of Mike Holt Enterprises 2008



CTA-ID : 2042979
Was this helpful?
What can we do to improve the information ?