Technical FAQs

Ask a Question

Can a QO112L200GRB, load center, be converted from a main lug to main breaker load center? What would the Catalog number be, to accomplish this?

The main circuit breaker to use to Convert this main lugs load center to a main breaker load center is Catalog number - QOM2200VH, which is a 200 amp circuit breaker.

CTA-ID : 2042597
Was this helpful?
What can we do to improve the information ?