Technical FAQs

Ask a Question

What are the catalog numbers and trip ranges for Powerpact H and J frame motor circuit protectors?

Issue:  
What are the catalog numbers, full load ampere ranges, and instantaneous trip setting specs for the Powerpact H and J frame MCPs for motor loads?  

Product line:  
Motor circuit protectors

Environment:  
Powerpact H and J frame MCP devices

Resolution:  
The following tables provide the catalog numbers, FLA, instantaneous trip ranges, and interrupting ratings for the Powerpact H and J MCPs.  




Note that all these options are also available in I-line construction.  You would order them with an "A" in the 3rd character place, for example:  HJA36030M71
Was this helpful?
What can we do to improve the information ?