Technical FAQs

Ask a Question

Will the QMB322HW accept the Class J fuses?

Issue:
Will the QMB322HW accept the Class J fuses?

Product Line:
QMB Panelboard, switchboard with QMB distribution.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The QMB322HW accepts only 240V rated fuses. Recommend using a QMB362HW, which will accept the 600V rated Class J fuses. The load base assembly will require repositioning in the field. Relocation holes are clearly marked in the switch.


CTA-ID : 2042119

Was this helpful?
What can we do to improve the information ?