Technical FAQs

Ask a Question

What size mounting bolt is used for the AL600LI7 lug?

This lug uses two 1/4 - 20 x 9/16 UNC bolts.


CTA-ID : 2041612
Was this helpful?
What can we do to improve the information ?