Technical FAQs

Ask a Question

What are the repair parts for the CH361AWC, series F5 (may be shown as F05)?

Issue:
Previous design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The repair parts for the CH361AWC, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly -40566-147-50 (requires one per switch. Arc suppressor assembly not included)
-Load Base Assembly - 40566-143-50 (requires one per switch)
-Line and Load Base Mounting Screw - 40205-151-01(3 for line & 2 for load)
-Arc Suppressor Assembly - 40566-355-50 (requires one per switch)
-Arc Suppressor Mounting Screw - 40205-145-01
-Handle/Mechanism kit - HMR0306FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL0306F (one kit includes all line and load lugs)
-Receptacle - 25410-02806
-Receptacle Mounting Screws - 45102-801-01 (required 4)


 
Was this helpful?
What can we do to improve the information ?