Technical FAQs

Ask a Question

Can a QOM2200VH MB be replaced with a QOM2150VH in a Homeline Load Center?

Issue;
Product Design Feature

Product Line:
QO and Homeline load centers

Evironment:
Main breakers

Cause:
Application

Resolution:
Yes. a lower amp, same frame size main breaker, can always be lower in the Load Centers, but not higher or increased.


CTA-ID : 2041242
Was this helpful?
What can we do to improve the information ?